Function principle


Electrode steam humidifier function principle

In a steam humidifier with dipped electrodes (isothermal humidification) water is heated to boiling point inside the cylinder to produce steam. The evaporated water is automatically refilled via the water supply network.

Isothermal humidification

Water is heated to boiling point inside the steam cylinder to produce steam. Voltage is applied to the dipped electrodes, so that electrical energy flows from them through the water to produce heat.

The strength of the current is purely a factor of the properties of the feed water. The more minerals there are in the water, the higher its conductivity and therefore the faster the required quantity of steam is produced.

Login on E-Stulz

for detailed technical specs

Contact us

STULZ GmbH
Holsteiner Chaussee 283
22457 Hamburg 

Central Office: +49 40-5585-0
Fax: +49 40-5585-352

Contact us
To top