Industrial Cooling
Air cooled scroll chiller with integrated Free Cooling
Sector: Industrial Cooling
Scope: Process Cooling
Requirements:
- Highest availability of the cooling system (all year round)
- Longest possible operation with Free Cooling
Description
The requirement for reliability was resolved by using two separate refrigerant circuits. In normal operation, both refrigerant circuits work using sequencing. If a compressor or a refrigerant circuit drops out, a minimum of 50% of total capacity continues to be available.
The chilling system was manufactured at our plant in Italy and delivered in one piece. Production and installation diagrams were planned in 3D and implemented on site. Soft starters were used to reduce the compressor inrush current.

Air cooled scroll chiller WPA
Technical Data | ||
---|---|---|
Cooling capacity Q0 | 302 kW | |
EER incl. chilled water pump | 3.00 | |
Refrigerant | R410A | |
Refrigerating agent | 70/30% water/glycol | |
Refrigerant inlet | +10°C | |
Refrigerant outlet | +6°C | |
Ambient temperature | +35/-20°C | |
Sound power | 79 db(A) | |
Compressor make and type | 2 x 2 scroll compressors |
To top