Please select your country

STULZ worldwide

Rotkäppchen Mumm

  • Rotkäppchen Mumm

  • CyberCool 2

  • 860 kW

  • Germany, Eltville

  • Sufficient reserves for fail-safe operation

  • Minimizing the noise of the running system

The Customer

Rotkäppchen-Mumm is Germany’s largest producer of Sekt (sparkling wine) and produces its well-known Rotkäppchen Sekt alongside spirits and wines such as Chantré, Echter Nordhäuser and Blanchet. With total sales in 2016 of around 271 million bottles of Sekt, spirits, wine and wine-based beverages, the company accounts for 55.4 % of the German Sekt market, achieving overall sales figures of 986 million euros.

The challenge
Our solution
The result
Our product

Rotkäppchen-Mumm needed a chilling system for the vacuum dealcoholizing process for the production of its alcohol-free alternatives, such as "Rotkäppchen Alkoholfrei" and "Mumm Dry Jahrgang Alkoholfrei", at its Eltville plant. However, the site is situated in the town’s historic center, right next to the banks of the Rhine. Rotkäppchen-Mumm therefore wanted to prevent noise disturbance to residents. So, the first challenge was to install a liquid cooling system that could provide the necessary cooling capacity and operational reliability, but with the lowest possible noise level.

The greatly fluctuating water flowrates posed a further challenge. The degree of required cooling varies greatly depending on the production phase, so that sufficient reserves are required for fail-safe operation.

 

.

In order to generate the required cooling capacity and satisfy the noise constraints, Rotkäppchen-Mumm chose a CyberCool 2 from STULZ with a cooling capacity of 860 kW. The unit’s "Axi-Top" fan diffuser attachments are specially designed to maximum efficiency while guaranteeing minimal noise levels. Moreover, deliberately oversizing the heat exchangers of the chiller allows the system to run at a reduced fan speed. This also has a positive effect on sound output. Another advantage of this oversizing is the increased energy efficiency and durability of the system, which covers approx. 70 % of production capacity even with a single refrigerant circuit.

 

To ensure fail-safe operation, the vacuum dealcoholizing process demands dramatically different water flowrates in the various phases. To meet this challenge, a 6 m³ buffer tank was designed and installed, to always provide sufficient water for each phase of the process. The tank and all pipework were constructed of stainless steel 1.4571 to AD2000. What’s more, the system features two redundant refrigerant circuits, each of which is equipped with a Bitzer screw compressor.

The chilling system was manufactured at STULZ’s Hamburg plant and tested on the company’s own performance testing station to ensure it met the necessary operating and design conditions. This considerably reduced time spent on start-up at the customer’s site.

Production and installation planning, including individual components and pipework, was all in 3D for greater peace of mind, and was performed on site.

Since Rotkäppchen-Mumm had purchased a turnkey solution, STULZ coordinated acceptance testing by the approved inspection agency and was continually at hand during this process.

CyberCool 2

Maximum energy efficiency and optimum reliability for complex, ambitious chiller solutions without compromise – this is what our CyberCool 2 chilled water systems stand for. And for a completely novel overall concept, whereby all the components of the CyberCool 2 are perfectly harmonized to ensure both high energy efficiency and low noise emissions. The result is a range of chillers that already meet the requirements of the Eco-design Directive 2021.

 

To the Product

Individual solutions with STULZ

You are looking for an individually configured solution for the efficient cooling of your project?

Our qualified experts will be happy to support you with an in-depth analysis and competent advice.

Get in contact