Please select your country

STULZ worldwide

Stadium Galgenwaard

  • Stadium Galgenwaard

  • Netherlands, Utrecht

  • STULZ Explorer WPA

  • Maximum performance in terms of efficiency

  • Environmentally friendly refrigerants

  • 504,3 kW

The Customer

FC Utrecht's 1st team is playing in the top-flight Dutch football competition (the 'Eredivisie'). FC Utrecht's stadium is called Stadium Galgenwaard. It was built many years ago and has been renovated several times. The last important renovation dates back to 2005. Large organisations such as FC Utrecht rely on high quality installations, including for the main building's cooling installation and its technical maintenance and implementation aspects.

For this project, Jadikoel took the initiative of examining the existing cooling system of the stadium's main building. 

The challenge
Our solution
The result
Our product

The issues became clear through temperature variations in the Stadium's main building. Jadikoel concluded these issues were caused due to the malfunctioning of the former unit (12 years old), installed on the stadium's roof. Simply repairing the unit was becoming too expensive and it could no longer be relied on.

STULZ joined forces with Jadikoel to deliver and install a new cooling unit for Stadium Galgenwaard.  

Jadikoel BV is a total installer and an all-round maintenance company specialized in air conditioning and climate control.

In the past, Jadikoel already worked on several other projects for Memid Galgenwaard and FC Utrecht, therefore the link was easily made. Jadikoel was founded in Nieuwerbrug in 2000. Flexibility, quality and service are the company's key focus points. Together, we aimed to provide the best service and highest quality for our client. We reinforced each other where necessary. Jadikoel clearly demonstrated that knowledge, design, installation and assistance for these types of complex installations are all available in-house.

To resolve the issue of temperature variations, STULZ suggested an air-cooled cooling unit, manufactured by STULZ, Explorer WPA180SCNA type, suitable for outdoor installation. This solution ensures a proper regulation of the main building's temperature, without any undesired variations.

The cooling unit has 6 suction-gas cooled hermetic scroll compressors in two refrigerant circuits, with a 6-level capacity control. The maximum cooling capacity amounts to 504.3 kW, cooling 86.51 m3/h of 12 °C water to 7 °C, in an ambient temperature of 35 °C. 

The used refrigerant is the environmentally friendly and highly efficient R410A. The aluminum Microchannel condensers are set up in V and are provided with 8 AC axial fans for an optimum heating output to the outside air.

STULZ Explorer WPA

The STULZ Explorer Line is a series of air-cooled chiller systems that is suitable for numerous different uses. The units of this product series combine high-quality components with the ability to fulfill project-specific requirements. We offer a portfolio of state-of-the-art industrial water chillers that are kind to your budget and flexible enough to be adapted to all customer requirements.

 

To the Product

Individual solutions with STULZ

You are looking for an individually configured solution for the efficient cooling of your project?

Our qualified experts will be happy to support you with an in-depth analysis and competent advice.

Get in contact